This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2904-Q1: pin current

Part Number: LM2904-Q1

Hi experts,

What's the current capability of the IN+ and IN- pins of LM2904AVQDRQ1? Thanks.

Arie

  • Hello Arie,

    The data sheet doesn't allow any current because the input range is limited to -0.3V to 26V as an absolute maximum range. In this range, no current flows.

    At the customer's risk, up to -10mA is believed to be damage free. However up to -1mA would be better. The op amp may go into phase reversal during this negative input current time. There is no input diode to V+ so input voltage should be less than 26V