I suggest clarifying the TLV906xS data sheet concerning the pin connections. It is indicated that one should connect the thermal pad to V_, but it is not clear that the device is inoperable unless this connection is present. It is stated that the thermal pad is important for thermal and mechanical stability, but it is ambiguous whether it is essential for electrical operation. I discovered this while prototyping a design with a QFN breakout board that refused to operate correctly. Using a breakout board with vias under the thermal pad provided the necessary electrical contact point and resolved my problem. I'd recommend that this be spelled out clearly in the data sheet (specifically: an external connection from V_ to the thermal pad is MANDATORY) to save others from the lengthy troubleshooting I went through.