Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G38DBVR.
Please refer to the below image.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G38DBVR.
Please refer to the below image.
Hello Anusha,
Is this request for LM7301IM5/NOPB or SN74LVC1G38DBVR?
Hi Ron,
Sorry of the in convenience caused.
Please note it is requested for LM7301IM5/NOPB
Hello Anusha,
Welcome to e2e!
I used the moisture sensitivity level search:
To help interpret the MSL, please use the following resources:
MSL Ratings and Reflow profiles
Recommended Soldering Profiles
J-STD-020:J-STD-020E.pdf
All the best,
Carolina