Other Parts Discussed in Thread: LMV821-N
Hi
Please help confirm whether LV9051IDCKR is suitable to replace LMV821SQ3T2G, Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The cross reference tool says that the TLV9051 is a drop-in replacement.
The LMV821-N web page says that the TLV9051 is a "Drop-in replacement with upgraded functionality to the compared device."
Hey Gareth,
Please see the below table for a comparison between the LMV821 and the TLV9051. I checked the page, however, and noticed that the DCK package is out of stock. Could you provide system specs or a circuit so I may help you find a device in stock that meets your system requirements?
► Part Number | LMV821 | TLV9051 |
Channel Count | 1 | 1 |
Vs Range | 2.5V to 5.5V | 1.8V to 5.5V |
GBW (MHz) | 5.5 | 5 |
Slew Rate (V/µs) | 1.9 | 15 |
Vos max @ 25oC (mV) | 3.5 | 1.6 |
Vos Drift, typ (µV/oC) | --- | 0.5 |
Rail-to-Rail | In to V-, Out | In, Out |
IQ typ (mA) | 0.3 | 0.33 |
VN (nV/√Hz) | 16 | 20 |
ISC typ (mA) | 56 | 50 |
IBias (Max) (pA) | 120000 | --- |
Operating Temperature (°C) | -40 to 125 | -40 to 125 |
Best,
Jerry
Hey Gareth,
The slew rate of TLV9051 is faster than LMV821. Could you help me help you by providing some more information on the application so I can find you a good alternate part?
Helpful specs would be (but are not limited to)
Without knowing about the application, the best I can provide you is a list of parts we have in DCK package.
https://www.ti.com/amplifier-circuit/op-amps/general-purpose/products.html#~p2954=SC70
Best,
Jerry