Hi team,
When reading the following linked documents, there are two questions:
https://www.ti.com/lit/an/sloa011b/sloa011b.pdf
1. VO ≤ + VCC – VR1 – VBEQ6 – VSATQ6 and VO ≥ – VEE + VR2 + VBEQ7 + VSATQ7
Isn't the saturation voltage drop of triode VCE voltage? If so, the VBEQ voltage should not be subtracted
2. Why the maximum value that VBQ6 can reach is +VCC? There is a current source between VCC and VBQ6
Best Regards,
Amy Luo