This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903B-Q1: LM2903BQPWRQ1 max value of the t_response

Part Number: LM2903B-Q1


Hello team,

could you please tell us max value of the  the t_response?

i can only find typ value.

best regards,

suzuki

  • Hello Suzuki,

    Since max response time is not in the min/max column, we cannot provide a limit.

    Propagation delay was extensively characterized over supplies, temperature and input overdrive, as shown in the graphs on page 13 (Figs 31 through 36).

    We would recommend that they look at the graph that is close to their supply voltage, temp range and input overdrive, and take the worst case value and add 30% for variation.

    If you just take the worst graph on the page at 1000ns, that would be 1.3us. For design guidance, I would use 1.5us max for a comfortable margin.