I use the LM6211MF as a buffer for my reference voltage. It is supplied with ±5V from a DC-DC converter. On the output there is a 2.2uF and a 100nF . This is workin for years, now we change the input in DC-DC and the
supply is rising much slower. In this case the output and input of LM6211 are going to +5V.
How can I solve the Problem?
Do I need to change the OP AMP. This is the simplest solution or do I need to adjust the circuit?
The body of LM6211 is SOT23-5.
Thank you for help.
Rubin Müller