This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: Differential drive vs single-ended drive

Part Number: LMH5401
Other Parts Discussed in Thread: LMH3401

Hello,

I am wondering if a 50Ohm 1:1 transmission balun in front of the LMH5401 would improve its distorsion performance? 

In that case the LMH5401 is driven differentially with an equivalent 25 Ohm for each single-ended source.

Almost all the datasheet covers the single ended to differential configuration. 

Any input concerning the benefit of the LMH5401 differential drive would be appreciated.

Thanks,

Nicolas