Other Parts Discussed in Thread: TINA-TI
Hello,
I was using the OPAX205A Pspice model found in sbomb98a.zip and the input bias current seems to be much larger than stated in the OPA2205 datasheet. Instead of the expected 0.1nA, the model produced around 50nA, increasing the total offset significantly when used in a typical circuit.
I looked inside of the model, and on lines 157 and 158, what seems to be the input bias currents are defined to be 50nA for each input terminal:
I_IBN MID ESDN DC 50N
I_IBP ESDP MID DC 50N
I edited these lines to set the values to 100pA each, and the model now produces the expected (typical datasheet) value of 0.1nA input bias current. However, I did not model the input offset current, or do a clever estimation of the input bias current differences between input terminals, so if there is a more realistic value to use for each input terminal’s bias current, I would appreciate knowing those values.
Thanks!