Part Number: TLV3605
Hi,
I would like to check is it valid to configure the hysteresis voltage by using an external voltage instead of resistor. The datasheet doesn't mention controlling with external voltage but the simulation model do include this as note. The simulation model is saying by inputting 0.8V to 1.25V at LE/HYST pin can create a hysteresis voltage of up to 60mV. Is this valid?
Thanks.