Other Parts Discussed in Thread: LM2903
Team,
I'm assuming that the LM2903's output is high impedance when unpowered, but don't have one here in the lab to double check. Can you please confirm?
Thanks!
Greg
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes. When VCC is at 0 V, then no current can flow into the base of the output transistor, and it is off.
Hello Greg,
Yes. As Clemens said, the output device is a transistor with no base drive - but there may be some tiny nano-amp level leakages to GND and/or Vcc. The pins do not have upper ESD clamps to Vcc, so the inputs and output can be taken up to 36V without damage, even when Vcc=0V. With the common pull-up resistor values...you probably won't even notice a difference between powered and un-powered.
Vcc=0V is not a valid operating condition, so leakages are not not characterized..
Thanks Paul, I appreciate the confirmation that there is not a leakage path from the output that may bias on the transistor. That was my concern!
Regards,
Greg