Other Parts Discussed in Thread: INA240,
Hi Current Sensing Folks,
Does TI have p2p device for INA282AIDR? Otherwise, could you help suggest any similar device even though it's not p2p? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ella,
For possible pin to pin replacements for the SOIC version of the device (D), I would recommend looking at the automotive version, the INA282-Q1, as well as the INA240.
Note that the INA240 is not functionally equivalent, and the customer would need to ensure that the device will fit their application. For example, the INA282 is capable of up to an 18V supply, while the maximum supply available on the INA240 is 5.5V.