Hello,
I have USB2ANY interface and BQ79656EVM device.
In the description of AutoEval GUI software for programing the BQ79656EVM, I see these instructions (page 5, 1.1.3 Updating USB2ANY Firmware):
"This step is crucial to having the GUI work correctly without any errors, and may be the first issue if you run into
any problems when first connecting to the EVM. If you do not do this correctly, the GUI will notify you that either
your USB2ANY Hardware is not connected properly or that you have an outdated firmware version. If the GUI
recognizes this, it will prompt you with the latest firmware and further instructions to update the USB2ANY.
1. To properly use the latest bqAutoEval PG2.0 GUI v1.0, you are required to update to firmware version
3_1_1_14. This file is named USB2ANY_3_1_1_14 - BQAutoEval.txt.
2. Download and extract the contents of the USB2ANY Explorer installer folder (2_slvc695.zip, this can also
be downloaded from http://www.ti.com/tool/USB2ANY and downloading USB2ANY Explorer Software under
Key Document) and run the executable from within it. Keep all default installation folder locations.
3. To update the USB2ANY firmware,ensure you have downloaded the USB2ANY SDK and ran the executable
(2_USB2ANY_2.8.2.0_SDK_Setup.exe). If the default location from the installation wizard was not changed,
the folder can be found in C:\Program Files (x86)\TI USB2ANY SDK.
4. Ensure the USB2ANY firmware file "USB2ANY_3_1_1_14 - BQAutoEval.txt" is saved somewhere to the hard
drive. Copy the "USB2ANY_3_1_1_14 - BQAutoEval.txt" file and paste it into the Firmware folder as in the
below image."
But both of the files "USB2ANY_3_1_1_14 - BQAutoEval.txt" and "2_USB2ANY_2.8.2.0_SDK_Setup.exe" are not available to me. I cannot find them on my computer.
Can you help me find them?