Hello,
I was looking into the input offset voltage rating over the temperature. So if I take the example of TLV9002, the datasheet says that on normal conditions max is +/- 1.6mV and over a temperature range, max is +/- 2mV.
The Vos vs Temperature value is given as +/- 0.6uV/C. So if I use this value to get max offset voltage at 125C, it will come out as 1.66mV(I am assuming that it will increase with temperature). So this calculated value and the given value are not matching and there is a significant difference.
Am I missing any point here to consider when calculating the offset voltage? Is it linear with temperature?
Best regards,
Lucas Pucheta: AFAE