Other Parts Discussed in Thread: OPA2348, , OPA2379, TLV9002
Team,
Because of availability issues and in order to migrate between possible alternatives (OPA2348 <-> TLV9042, OPA2379 <-> TLV9002) :
-From the PCB footprint point of view are the SOT-23| 8 and SOT-23-THIN|8 package 100% compatible?
-Can a PCB for SOT-23|8 (OPA23xx) be used as is for SOT-23-Thin|8 (TLV9xxx)?
-If not can you make suggestion to accommodate both using the same footprint geometry?
Thanks in advance,
A.