This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM111QML-SP: 28VDC supply Voltage

Part Number: LM111QML-SP


Hello,

Would the LM111QML-SP work with a 28VDC supply voltage? The datasheet says 5VDC to +/-15V , but it also says it should be able to switch up to 50V and the positive supply voltage is up to +30V.

Thanks

  • Hello Horace,

    Yes. It can work with a single +28V supply. The abs-max table shows the various limits as to how far the voltages between the various pins is possible. At +28V, you are fine.

    Just beware that the valid input range is +0.5V to +26V on a single +28V supply.