As I read the datasheet, current sensing of I*R less than 20mV cannot be expected for low voltage supplies when VCM is less than or equal to VS, the supply voltage (Section 7.4.2.4).
Is that correct?
I am trying to evaluate using the part for low voltage supplies (3.3V, 2.5V 1.8V, 1.5V) that are more sensitive to series voltage drops and can have a wider range of operating currents. If my understanding is correct it would limit the useful application to 20mV < I*R < Vmax, where Vmax is the highest voltage drop that can be tolerated for the power supply output.
If true I will need to look for other 50kRad tolerant options.
Thanks