Hello guys,
One of my customers is evaluating OPA2376 with low pass filter circuit like the follow.
https://www.avrfreaks.net/forum/why-simple-op-amp-low-pass-filter-does-not-work
The customer parameters are the follow.
R1 = 1k ohm.
R2 = 68k ohm
C = 0.01uF
But they want set the filter cut-off frequency lower than the above.
At this moment, they have the following question.
Q. What is the maximum capacitor value can be driven by OPA2376 for the low pass filter circuit?
Your reply would be much appreciated.
Best regards,
Kazuya.