Other Parts Discussed in Thread: LMV321-N, , LMV321, TLV9001, TS321, , OPA990, OPA170
Hi All
I have having difficulty locating a supplier for the LM321MF SOT-23
Is there a newer alternative component available with the same package?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In a low-voltage circuit, consider the LM321LV, LMV321, LMV321-N, or TLV9001U.
Most other SOT-23 opamps have a different pinout.
Hi
Thanks for the information
I cannot find any texas instruments components available
The only produxt I can find in stock is the LMV321RILT
Would this be OK?
The LMV321RILT is made by ST, and the "R" means that it is a variant with a different pinout.
Apparently, some LMV321Q3M5/NOPB are available.
Hi Chris,
Did you look at TI.com for any alternative parts? Our product search allows you to see whether we have inventory or not. More details on how to use this feature and others can be found here: How to Find In-Stock Alternatives.
It won't be able to tell you if the pin outs are different or not but it should help narrow down the search.
Best Regards,
Robert Clifton
Here I tapped into an old parametric database I had, this has no package info and the pricing is old - but these parts overlay the parametrics of the LM321 ok - so these, I think, would be safe drop ins but you would need to confirm package and pricing. The LM321 is ancient, but has a great price - but if you can't get it, might not be the most important parameter. After a bunch of sorts for overlapping parametrics, this final list (from an initial >1200 lines for TI and NSM <50MHz BW parts) is sorted in ascending price.
The OPA170 looks pretty interesting, but - amazingly it is also apparently out of stock - that part does list an upgrade in the OPA990 that was not in my older database, It is a pretty good price, but also out of stock it seems right now.
You may have to expand your search outside of TI for this older LM321 equivalent.
Unfortunately, the LM321 in SOT-23 uses a non-standard pinout. The only pin-compatible alternatives either are called "321" or are explicitly designed as a replacement (like the U variant of the TLV9001).
Well actually, that OPA170 offers what looks like a pin compatible SOT23-5 in the DRL package - and, it now appears to be shortly available!!
I wouldn't want to solder SOT553 (0.5 mm pitch) onto a SOT23-5 footprint (0.95 mm pitch).
I see, it looks like the pin rotation is correct - and could sit inside the larger DBV footprint if desperation demanded. But not an easy solution.
Hey Chris,
If any of these answers solved your question, please mark them as resolved! Otherwise I'm going to close the thread.
Best,
Jerry