This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA860: best for generating a low amplitude (1 mA) sinusoidal current between 50 - 100 kHz.

Part Number: OPA860
Other Parts Discussed in Thread: OPA861, OPA615, LM13700, OPA2210

Hi Team, 

The customer is working on a voltage-controlled current source and would like to use an operational transconductance amplifier (OTA) integrated circuit and they are requesting to know which part would be the best for generating a low amplitude (1 mA) sinusoidal current between 50 - 100 kHz.

I've checked our products and found the OPA860, OPA861, and OPA615. Will this device work? if not, can you suggest a device?

Thanks and regards,

Marvin