Other Parts Discussed in Thread: LMH6723, , LMH6609
Dear Sir,
I design a 10 MHz distribution amplifier with a band-pass filter at the input. I used the THS4271 amplifier to build the filter, and the LMH6723 amplifiers for the output stages. I tested circuit with an Agilent 33250A generator with the following settings:
- Amplitude: 3Vpp
- Offset: 0V
- Frequency
- 10MHz
- Shape: Sine
The THS4271 chip gets very hot. Putting your finger on the chip (taking the temperature away) improves for a while. In addition, the amplifiers on the output stages also introduce distortions, despite the fact that they work with a gain of 1. The filter circuit was taken directly from the Texas Instruments book:


I also send photos and gerber files of the PCB. Is the problem an incorrectly designed board? I also attach a photo from the oscilloscope with a distorted signal. I am asking for help, because I do not know what the problem may be.