This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL391B: leakage current when VCC=0V but V+ =12V

Part Number: TL391B
Other Parts Discussed in Thread: TINA-TI, LM339

Hi Team,

Our customer is using TL391B for power detection, V+ is connected to 12V battery pack anytime, VCC=15V comes from adapter, V- is resistance divider of VCC. If 15V adaper doesn't present, the TL391B would not get the power, so we wish TL391B not work in here. But we are wondering the leakage current at V+ pin. 

We use TINA-TI to simulate the situration, V+ leakage current seems fine, but we note the VCC leakage will up to 550uA, that's un-acceptable in battery pack application. Could you help to confirm the leakage current 550uA is correct? thanks.