Hi folks
I have designed a circuit to measure low currents such as 15uA using INA190. However, I am having an issue when I tray to disable the IC. I will try to explain.
Initially, the circuit is as following:
When I apply 3V3 to Csense, I can measure the current across R14.
The problem is when I try to disable U4. If I pull Cs_EN to zero, apply 3V3 to Csense, I am getting 2.8V at IN- pin.
I even tried to remove R14, and the voltage at IN- still at 2.8V.
I also tried other drastic test: I removed R12, R13 and C8, disabled U4 pulling pin 2 to low, and still measuring 2.8V at pin 8.
The IC is not damaged, because the same behaviour happens when I change IC or try another PCB.
Does someone have a clue on this?
Thank you