Other Parts Discussed in Thread: INA148,
Question from customer regarding the differences between INA148 and INA148-Q1:
what procedure is used to designate storage temperatures since they appear to be different:
INA148QDRQ1 = -65°C to 150°C
INA148UA/2K5 = -55°C to 125°C
What exactly is affected by long term exposure? Electrical specifications or packaging deformation/damage?
Is this a typo on the -Q1 data sheet or does it really have the lower storage temp? If so, why? seems like a odd value.
Thanks!
-Steve