Hi Expert,
My customer has a new requirement for the EC mirror control which list as below.
Requirement:
- dual output,
- Output range: -1.25V~1.25V, 0.1V~0.2V step, ±0.2V accuracy per step
- output current: 500mA
I would like to check if ALM2402-Q1 can meet this requirement? Does ALM2402-Q1 can connect negative power rail to GND pin?
Thanks!
Ethan Wen