Part Number: INA200
Hello,
I am using the INA200 chip as a high side current monitor after the switching FET as shown in the attached schematic.

The issue occurs when we short circuit out1 to battery (27V). We have no issues with a short circuit to ground (which I thought would be the tougher of the two). After the battery short circuit, the INA200 does not read current correctly and we get false faults when a load is attached. If no load is attached, the circuit works okay (no fault). We have replaced the chip and verified it was the chip causing the issue. We added the 220 Ohm resistors (R15 and R16) in series with the sense lines and that let us short circuit up to 30V successfully. We don’t want to increase the resistance too much, as that effects the gain and accuracy of the chip. Any suggestions would be appreciated. We are in the process of monitoring the Vin+ and Vin- lines with an oscilloscope during a short circuit to see what they look like.