This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2336: GBWP of OPA2336

Part Number: OPA2336
Other Parts Discussed in Thread: OPA336, OPA391, OPA392

Hi Team,
I want to measure the current through a resistor that is connected to the low side.

The Resistor R13 (2E) is the sense resistor.

The H Bridge is switching at 22KHz.
The expected current through the sense resistor is 100mA.
So the voltage developed across the resistor will be 100mA*2E=200mV.
I need to amplify this 200mV to about a 3V range, so I need a gain of approximately 10.
The feedback resistor of the op-amp OPA2336 is taken as 100K and the gain resistor is taken as 10.5K.
The Gain-Bandwidth Product of OPA2336 is only100KHz.
The H bridge is switching at  23kHz, since the current sensing is outside the H-bridge, the current signal is rectified to 46kHz.
Maximum amplification will be 100KHz/46KHz = 2.17
My required amplification is 11.
Is my calculation correct?. Please correct me If I am wrong.
Could you please explain the relationship between the GBWP and the maximum input frequency of an op-amp?.