Other Parts Discussed in Thread: TINA-TI
Hi Team.
I am designing a temperature sensor with a 10K NTC.
Attached is the schematic as per the application note SBOA323A.
My required output voltage is from 0.5V to 3.2V.
The op-amp is supplied from a 3.3V voltage source.
My temperature range is 0°C to 50°C.
According to the datasheet of the NTC.
The resistance at 0°C is 26 783Ω to 27 913Ω
The resistance at 50°C is 4079.2Ω to 4237.3Ω.
Is my design correct?.