Part Number: TLV9151
Hi,
From the datasheet as shown below, does the highlighted statement means that the signal input pins are allowed to exceed (V+)+0.5V if the current is <10mA?

In my design, the supply voltage to TLV9151 is 5V. However, we realized that the signal input may have the risk of exposure to a voltage of 6V. This line has a 150kOhm current limiter in front so the current is very small. Will it still damage the TLV9151?
Thanks.