Other Parts Discussed in Thread: INA149, OPA392
Hi everyone,
I am trying to design a high voltage sampling system as part of a larger project.
The sampling front end will eventually drive a AVR128DA 12 bit ADC.
ADC reference will be 1024mV.
Given the chaos of the IC shortage and the need for lowering cost per project unit i am searching for a solution in measuring the 230VAC with the uC ADC above.
So, using Tina i was able to put together the circuit given below:
Everything looks great but i have some concerns regarding the GND of the AC.
What if the system ground is connected to the AC GND?
I grounded the Neutral (if i can call it that) of the AC source as you can see below:
But the simulation is not looking good:
Should i be using one of those high common voltage opamps like INA149? Still INA149 has a CMV of +/- 275V. Not sure what applies in this case, that is, high voltage sampling especially is the sys ground is connected to AC GND.
Can you pls help?
Maybe propose an better topology for high voltage sampling?
Thanks
Manos