Part Number: ISO224
Other Parts Discussed in Thread: AMC1302, AMC1300, AMC3302, AMC3301, INA149, AMC1336, AMC3330, AMC1350, AMC1351
..
Hi,
I am not able to find common mode voltage range for ISO224 in the datasheet. I want to use it for 900V System as a high side current measurement with shunt, can this chip handle high common mode voltage ? VDD1 and VDD2 will have more than 2kV isolation from my low voltage power supply. I thought the max common mode this chip can handle is probably VCC/2 like 6V. Do we need VDD1 and VDD2 both isolated wrt to 900V in order to make this work?
I am not sure whether this chip is meant for high side sensing for high voltage application, I see some high common mode voltage, isolation amplifiers are huge in size as against this for example AD210. Please comment.
Thanks,