Hi Expert,
I'm using below circuits to simulation with INA240A4.
The input is 10mV, 320kHz half-sinusoidal signal, however the output is very weird. There are mainly 2 issues:1). the valley value of out put signal is too far from zero. 2) There is phase shifted between input a nd output signal. Do you have any idea about what causes these abnormal output signals? Thanks.
Regards,