This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM393: LM393B issue

Part Number: LM393

Dear Team,

Our customer have an OPA(LM393BIDR) issue as below, please help to check if the design is ok.

 

 

 

 

 

When DCIN_27V_1 greater than "V+",  the pin1 will output "Hi-Z".

When DCIN_27V_1 less than "V+, " the pin1 will output "0".

 

But we found that some PCBs behave abnormally

Channel 1 : Pin1 (3.205~3.245V)

Channel 2: Pin2 (2.449~2.482V)

Channel 3: Pin3 (2.365~2.43V)

Many Thanks,

Jimmy