Part Number: TLV3502
Hello,
I just want to confirm that these two devices (TLV3502 & TLV3502-Q1) are the same silicon, the Q1 just has additional testing for the automotive qualification.
Thanks,
Nick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV3502
Hello,
I just want to confirm that these two devices (TLV3502 & TLV3502-Q1) are the same silicon, the Q1 just has additional testing for the automotive qualification.
Thanks,
Nick
Hello Nicholas,
Yes, they both use the same die revision, fab code and die sizes, though the die ID are slightly different (this is not unusual for Q1 devices - as Q1 devices are tracked differently), so I cannot say they are exactly the same - but they seem to be.
The assembly flow and package BOM are slightly different, as is common with commercial and Q1 sister devices. I cannot get into the differences in a public forum.
Functionally and electrically, they are identical.
Nick
thanks for your support of the forum. I believe your question has been answered, so I am closing the post.
Chuck