Part Number: TL082B
Other Parts Discussed in Thread: TL082,
Team,
Can you please help with the below?
TL082 is being used for some years in an existing design.
The below issues has just raised during production with a specific lot of TL082B.
7500u have been soldered and so far 70 board do show this behavior (which gives a very high PPM failure).
According to the data sheet, the TL082B should have a maximum offset (VIOmax) of 3mV.
Together with the amplification specified by the circuit (Vu=10), a maximum voltage at the output of 30mV should result at 0mV at the input, but usually the values are more in the range of 10mV.
During test an output voltage of up to 100mV was measured with a with Tektronix DPO 4104B.
The schematics and measurement points are given below.
-Can you please help to debug the issue?
-What can we test/check in our HW in order to find the root cuse?
-Are the been some changes in the TL082B TI production test?


Thanks in advance,
A.