This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903: Maximum voltage that can be input to the IN+ pin

Part Number: LM2903

Hello,

What is the maximum voltage that can be input to the IN+ pin when the customer uses the LM2903 under the following conditions? Can it be used up to +30V?

   - VCC = +5V

   - IN- = +2.5V

Thank you.

JH