This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV7031: Zero crossing detection is not at 50% duty cycle

Part Number: TLV7031
Other Parts Discussed in Thread: TLV3491, TLV3201, TLV7011, LM393-N, TLV9031, TLV9032

Hi,

i built a 60 Hz zero crossing prototype circuit for 220 VAC mains power, but the output of TLV7031 comparator are not at 50% duty cycle.

I tested with TLV3491(i have this in my inventory) too and same problem.

I wanted to test with TLV7011 or maybe TLV3201, but TLV7011 i dont encounter($5 in some place) and texas instruments dont provide samples to Brazil anymore.

Input Positive cycle = 8,33 ms 

Input Negative cycle = 8,33 ms

Output Positive cycle = 8,42 ms

Output Negative cycle = 8,26 ms

What may be the problem ?

offset ?

Internal hysteresis ? But TLV3491 does not have hysteresis, only TLV7031 !!!

 propagation delay of only 3 µs ?

Is there a (simple) solution to get 50% duty cycle ??

Thank's.

Video:

Blue = positive comparator input(vi+), vi- is at ground

Yellow = comparator output 

https://youtu.be/yOmY0KqYAZA