Other Parts Discussed in Thread: OPA397, OPA396, OPA392, OPA391, OPA320, OPA196, OPA325, OPA191
Hi Team,
I have two question want to ask.
Can the op amp be used as a comparator?
Can the tlv4333 op amp be used as a Hysteresis comparator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
this thread may interest you:
Kai
Even though op amps output transition from one rail to the other may be 100-1000 times slower than comparators with similar quiescent current, one could use them as comparator BUT only if they have no back-to-back protection diodes between the input terminals. For this reason you should NOT use TLV4333 as comparators but instead you could use OPA391, OPA392, OPA396, OPA397, OPA320, OPA325, OPA191 OPA196, or any other op amp, which do NOT have those diodes.