Other Parts Discussed in Thread: TLV9002, , TINA-TI, OPA376
Ciao,
I just implemented 20 PCBs based on the sboa247 application note, but using the below values (based on the schematic at page 1):
IC = TLV9004IDR (SOIC-14)
V+ = Vex = 3.3 V
V- = 0 V (GND)
Vref = 574.6 mV
G = 434,65 V/V
R11 = 93.1 Ohm 1% tollerance
R4=R2 = 20 k Ohm 1% tollerance
R2=R3 = 4.99 k Ohm 1% tollerance
R8 =17.4 Ohm 1% tollerance
R5=R6=R7=R10 = 350 Ohm --> Strain gauges full bridge
R9 = 23.2 Ohm 1% tollerance
The circuit simulated in TINA-TI (with the TLV9002 op. amp. instead the TLV9004) works fine.
My problem is the output offset with zero input voltage from the Wheatstone bridge. Below you can read the measured values of "Vo - Vref" in the 20 PCBs (in milli Volts)
-387,6
-266,6
-249,6
-199,6
-141,6
-109,6
-107,6
-104,6
-64,6
-41,6
7,4
20,4
162,4
179,4
251,4
445,4
494,4
529,4
617,4
710,4
My questions are:
- Do you think the TLV9004 is the wrong component for this applcation ?
- In the application note, you set the gain at 1001V/V using the TLV9002, how big was your output offset error in the sboa247 application note ?
Thanks in advance for your help,
Marco