This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM119QML-SP: 5V Supply tolerances

Part Number: LM119QML-SP


Hello,

I'm currently validating a space card that will contain LM119QML-SP. We would like to know the tolerance for a 5V supply. Is it 5V minimum minimum or there is a small tolerance around this supply.?

Thanks.

Thibaut Gantner

  • Hello Thibaut,

    TI just specifies the specs at 5.00V for any limits.

    While not specifically mentioned, the designers at the time (1969) most likely allowed for the ±5% regulator tolerance of the time.

    Of course, TI recommends 5V or more..

    My *guess* is that it will most likely work down to 4V, but speed and bias currents will be affected.

    But be very careful of the input voltage range, as this is NOT a ground sensing input and has both upper and lower input votlage limits.

    For a single +5V supply, the input voltage range is +1V to +3V, and operating outside this can cause improper outputs. The upper range will decrease as the supply voltage decreases (Vcc-2V).