Other Parts Discussed in Thread: LM139-N
Hi Experts
Can someone provide the test configuration used for Figures 4 & 5 in the data sheet?
I’d like to know the input wave forms for both inputs.
Thanks!
Jim B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
more details are given in the datasheet of LM139-N.
See also this thread:
Kai
Thanks Kai. That previous post is a great resource.
Jim
Thanks for your post. In short those curves are created with VCC = 5V and a VCM = 2.5V. Underdrive is held at 100mV for varying OD levels. Pull-up resistor of 5.1k to 5V. The full description can be found at the post Kai pointed you too.
Chuck