Other Parts Discussed in Thread: TLC374
Hi TI Experts
When I use LM339APWR ,12V VCC, and the positive Input 5V as reference voltage, and how to make sure the propagation delay time? use the max 1.3us as the worst case propagation delay time as the datasheet? how to make the propagation delay time less or that to say ,how to make the comparator operate faster?
(1)The max propagation delay time 1.3us
(2)How about the high temperature such as 65℃ Ambient temperature that influence the propagation delay time?
Thank you very much!