This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP8645: low side current sensing with input filter

Part Number: LMP8645


Hi there,

I am using LMP8645 for a low-side current sense application as shown in the attached schematic. The current is a high-frequency diode-rectified unipolar current and I am trying to get the average of it. Therefore I have used an input filter.

1. The datasheet says that the input filter resistor can not be more than 10 ohm - is that for each input line? I have used 10 on each input line - is that ok?

2. The datasheet also says that the LMP8645 has an internal output buffer able to drive a capacitance load up to 30 pF or the input stage of an ADC. I am using the LTC1864 ADC, whose input impedance is not known to me. Is an output filter with 1k resistor and 180p capacitor as shown going to be a problem?

3. I am expecting to sense a max of 10A current, which means the common mode voltage will be -75mV. Therefore I am using Rg = 50k as per the datasheet recommendation. Is this ok?

4. The online error calculator on the product webpage shows more than 20% error for 1A sensed current. Could it be that bad? Please see the screenshot showing the values I put.

Thank you very much!