This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3302-Q1: High Side BMS Shunt Current Measurement

Part Number: AMC3302-Q1
Other Parts Discussed in Thread: ADS131B02-Q1, ADS131B04-Q1, ADS131B26-Q1

We are trying to design an isolated current measurement design based on a shunt measurement principle for high battery charge and discharge currents. The design should feature digital signal transmission to a master MCU, preferably via CAN. The AMC3302-Q1 could be a starting point for the design, but i wondered wether there is a more comprehensive solution to this problem.

With our power loss requirements (see below) the input voltage range of the AMC3302-Q1 is not favorable. We would not be using the full range when using a small shunt resistance (25µR to 35µR), therefore sacrificing resolution.

We would like to meet the following specifications for our measurement:

 

Parameter

Value

Unit

Nominal Measurement Range

±500

A

Power Loss (Shunt)

<9

W

Total Accuracy

±0.4

%rdg

Offset

75

mA

Linearity

0.01

% of range

Resolution

27

mA

Additionally we want to integrate various temperature measurements. Specifications on this still need to be worked out, but it may be relevant to an answer for the current sensing architecture.