Other Parts Discussed in Thread: AMC3330
Hi Team,
Good day! We need you help to check the customer's schematic.
Thank you in advance for the support.
Best regards,
Jonathan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Good day! We need you help to check the customer's schematic.
Thank you in advance for the support.
Best regards,
Jonathan
Hi Jonathan,
What type of application is this circuit going into?
I see that they are using an ADI opamp with extended temperature range, AD8479TRZ-EP, that operates from a minimum of 5V.
Do we have an alternative TI opamp that we can offer here?
Our HLDO_OUT voltage is typically 3.2V, so this specification will not be met and is specified to supply up to 1mA over temperature.
The resistor on the negative input, R245 is not necessary in this configuration, but will not affect performance negatively either.
Hi Alexander,
I was using AD8479 before AMC3301 because that don't have higher VCM. As I can't use AD8479 now, please suggest some other OPAMP with higher VCM or any other isolation amplifier with higher VCM (common mode voltage).
extended
Hi Gokul,
Can you please share some information about the application?
Is this for a current or voltage measurement?
What are the expected isolation requirements?
Why is a high common-mode voltage required?
Hi Alexander,
This is for a voltage measurement
Expected isolation requirement - Galvanic Isolation
The voltage which we are measuring is coming from a battery, for protection we require op amp with high common mode voltage.
Hi Gokul,
I recommend using the AMC3330 with a resistor divider then. An additional amplifier with a high common-mode voltage should not be necessary.
The AMC3330 is ideal for voltage measurements with high impedance resistor divider circuits and has with a larger input voltage range and higher input impedance compared to the AMC3301, which is primarily used for current measurements across low impedance shunt resistors.
The AMC devices themselves do not have high common-mode input ranges in the traditional sense. However the device has two grounds, high (HGND, pin 8) and low (GND, pin 9) side.
The INP/N input common-mode input voltage rating is the inputs (pin 6/7) with respect to HGND (pin 8).
The working voltage rating, is the maximum steady-state voltage difference between HGND and GND, 1.7kV_DC for the AMC3300.
Here is some collateral that may help: https://www.ti.com/lit/an/sbaa321/sbaa321.pdf
https://www.ti.com/lit/an/sbaa553/sbaa553.pdf
Please let me know if you have additional questions or would like a schematic review.