Part Number: THS4552
Hi everybody,
I have one question about configuring the input and output of THS4552PWEVM (https://www.ti.com/tool/THS4552PWEVM )
I have read the THS4552PWEVM guideline. The THS4552PWEVM board is designed for differential input to single-ended output.
However, My application is single-ended input to differential output singal with 1Mhz signal bandwidth.
How to configure the THS4552PWEVM board for my application?
My solution:
- At input: I terminate the IN1+ by 50ohm resistive SMA load
- At output: I remove balun and R14, add R1, R12=0 ohm, add SMA at OUT1 -
Could you please help me to solve this problem?
Thanks