This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA692: logic level square wave with G=1

Part Number: OPA692

Dear Technical Support Team,

I'd like to use 10MHz logic level square wave(3.3V and 2.5V etc from level shifter) with G=1.

I believe that OPA692 is better for this, although it's released 2002.

Do you have any other latest device  for voltage follower  and Video Amp, if you have ?

Best Regards,

ttd

  • Hi ttd,

    The OPA692 highlighted in our video amplifiers portfolio is the latest device with those characteristics. If your applications requires the features that make the OPA692 ideal for RGB line drivers such as the high output current drive with sustained bandwidth performance, then the OPA692 might be your best bet. However, if you don't require high output currents an amplifier not specific to video amps might work. May I ask what is your expected output load?

    Best Regards,

    Ignacio