Other Parts Discussed in Thread: OPA455, OPA454, OPA593
Hello,
I have been trying to find a replacement for the ADA4700-1 (first amplifier in the picture below) and the OPA462 seemed like a good fit as it shared the package, the high power supply voltage (+77V required) and most of the pinout (the OPA462 has an unconvenient Enable/Disable feature on pins 1 and 8).
Whatever I try, the power supply of +77V drops down to around +30V if the E/D and E/D Com pins are left open, or if I set up a voltage divider to have a +5V enable voltage between them.
Could anyone help me figure out what is wrong with my design using the OPA462 or help me find a replacement for that amplifier ? (I have not yet tried the OPA455 but being the same family of component I expect the same results).
Best regards,