Part Number: ISO124
Other Parts Discussed in Thread: ISO122, , AMC1411, ISO224, AMC1400
To Whom It May Concern
Hello, I've got a question about the component ISO124P. I’m utilizing this component for a project, but I found that the ISO124P has a small ripple noise and a small offset voltage in the output. I attached the images taken with the oscilloscope. The first image is the output of the ISO124P at 0 V.

I added the filter that the datasheet recommends, but the offset remains.

I would like to know If TI has identified the problem and has some solution for it, I’m sure that the offset is caused by the ISO124P because I tested the module without the ISO124P (without isolation), and this offset doesn’t show. The image shows the output of the circuit with the ISO124P and the filter that’s recommended in the datasheet (blue) and the circuit without the ISO124P (yellow).

Also, I attached the actual output of the circuit (blue) and the output of the circuit with the filter (yellow). In this example, I used another ISO124P because every ISO124P has a different offset and ripple noise. The offset in the first case was 2 mV, while the offset in this ISO124P was 18 mV.

I tried a pre-gain circuit that is recommended in the ISO122P datasheet, and it attenuated the problem but did not solve it. I would appreciate a solution for this problem because the hardware is entering into conflict with the software due to this offset. At last, I attached the output with the pre-gain circuit that recommends the datasheet of the ISO122 (blue) and the output of the circuit with the pre-gain circuit and the filter (yellow).