Other Parts Discussed in Thread: TL082
Hi Team
As the datasheet shows, input voltage range is Vcc-+2V.Can I understand that when the reverse pin(VF1) is lower than the voltage value, TL082H will work abnormally or even fail.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi kai
Thanks for your answer. As my simulation model, when VF1 is 0V and VF2 is settled from 10 to 100mV(lower than (VCC-+2V)) , the output of U1 is clamp to 27mV,whether it is make reason? And when I connect Vcc- to -12V, the output is consistent with the theoretical value, which V- and V+ meet datasheet requirment.
So can I think that TL082H is more suitable for power supply products powered by positive and negative voltage rails instead of single voltage rail?
Hi Nanxiao,
So can I think that TL082H is more suitable for power supply products powered by positive and negative voltage rails instead of single voltage rail?
Correct. The TL082H is no input-rail-to-rail OPAmp. If your input voltage goes down to VEE, then the TL082 is not suited in your circuit.
Kai